DTS for MicroChip KSZ9897 via RGMII?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DTS for MicroChip KSZ9897 via RGMII?

2,644 Views
syntech66
Contributor I

Has anyone had any luck connecting imx8 to a MicroChip switch like the KSZ9897 via RGMII?  We have been in an all out war for the past 2 weeks trying to make this work and I don't think we've progressed a bit.

The excerpts of our DTS are attached.  We are connecting ENET1 to port 6 on the KSZ, but we can't get the littlest bit of encouragement from everything we've read and done.  

dmesg looks like this:

[ 913.212173] imx-dwmac 30bf0000.ethernet eth1: validation of rgmii with support 00000000,00000000,00006280 and advertisement 00000000,00000000,00006280 failed: -EINVAL
[ 913.227388] imx-dwmac 30bf0000.ethernet eth1: __stmmac_open: Cannot attach to PHY (error: -22)
[ 913.251131] imx-dwmac 30bf0000.ethernet eth1: Register MEM_TYPE_PAGE_POOL RxQ-0
[ 913.259402] imx-dwmac 30bf0000.ethernet eth1: validation of rgmii with support 00000000,00000000,00006280 and advertisement 00000000,00000000,00006280 failed: -EINVAL
[ 913.274606] imx-dwmac 30bf0000.ethernet eth1: __stmmac_open: Cannot attach to PHY (error: -22)
[ 1214.051420] imx-dwmac 30bf0000.ethernet eth1: Register MEM_TYPE_PAGE_POOL RxQ-0
[ 1214.060102] imx-dwmac 30bf0000.ethernet eth1: validation of rgmii with support 00000000,00000000,00006280 and advertisement 00000000,00000000,00006280 failed: -EINVAL
[ 1214.075328] imx-dwmac 30bf0000.ethernet eth1: __stmmac_open: Cannot attach to PHY (error: -22)
[ 1214.099479] imx-dwmac 30bf0000.ethernet eth1: Register MEM_TYPE_PAGE_POOL RxQ-0
[ 1214.107759] imx-dwmac 30bf0000.ethernet eth1: validation of rgmii with support 00000000,00000000,00006280 and advertisement 00000000,00000000,00006280 failed: -EINVAL
[ 1214.122971] imx-dwmac 30bf0000.ethernet eth1: __stmmac_open: Cannot attach to PHY (error: -22)
[ 1214.147204] imx-dwmac 30bf0000.ethernet eth1: Register MEM_TYPE_PAGE_POOL RxQ-0
[ 1214.155488] imx-dwmac 30bf0000.ethernet eth1: validation of rgmii with support 00000000,00000000,00006280 and advertisement 00000000,00000000,00006280 failed: -EINVAL
[ 1214.170706] imx-dwmac 30bf0000.ethernet eth1: __stmmac_open: Cannot attach to PHY (error: -22)
[ 1214.194868] imx-dwmac 30bf0000.ethernet eth1: Register MEM_TYPE_PAGE_POOL RxQ-0
[ 1214.203148] imx-dwmac 30bf0000.ethernet eth1: validation of rgmii with support 00000000,00000000,00006280 and advertisement 00000000,00000000,00006280 failed: -EINVAL
[ 1214.218366] imx-dwmac 30bf0000.ethernet eth1: __stmmac_open: Cannot attach to PHY (error: -22)

 

Any suggestions or hints would be tremendously appreciated.

Thanks.

0 Kudos
Reply
1 Reply

2,617 Views
joanxie
NXP TechSupport
NXP TechSupport

you dts is limited, pls refer to the chapter 3.3 ENET FEC interface configuration of enclosed file, check if you set is correct or not

0 Kudos
Reply