DTS Codec for IMX6(d) processor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DTS Codec for IMX6(d) processor

5,631件の閲覧回数
gnanachandrandh
Contributor II

Hi There,

Is there DTS codec specific for IMX6D or IMX6 series processor? if so, where can I find it?

Is that a licensed software ?

Cheers

Gnana

ラベル(3)
0 件の賞賛
返信
3 返答(返信)

5,369件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI Gnanachandran

in last 3.14.28 FSL BSP release dts is supported as mpg2,mkv demuxer, not pure audio codec,

please check attached Release Notes Table 21. Parser/Demuxer supported audio/video,

Table 24. Audio codec specification

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

5,369件の閲覧回数
gnanachandrandh
Contributor II

Hi Igor,

Thanks for your reply.

I have few questions on DTS codec support for IMX6 in 3.10.17 FSL BSP.

  1. Does 3.10.17 FSL BSP  has  support for DTS codec for IMX6(D) ? If So ,Please share  How to verify it ?

  2.  if not (1), Can you share us link where we can find codec for 3.10.17 FSL BSP ?

  3. Can you please share us what are containers (like AVI, MP4, MPG2 , …)   supported by 3.10.17 FSL BSP for DTS codec?

  4. In our project, DTS codec support is required for .avi and .mp4. Are these two are supported in 3.10.17 FSL BSP ? 

   if not, What are the other possibility to achieve it ? (like limited version or licensed version)

Cheers

Gnana

0 件の賞賛
返信

5,369件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI Gnanachandran

please look at attached Release Notes what is supported in 3.10.17 release,

User Guide describes building steps.

In general if smth is not supported, custmer has choice to develop own solution using

Freescale Professional Services

http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_PROFESSIONAL

Best regards

igor

0 件の賞賛
返信