DSP can't ouput debug log on IMX8MP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DSP can't ouput debug log on IMX8MP

2,182 Views
jimmyli
Contributor V

Hi,

      We are trying to run HIFI4 dsp on IMX8MP, but encounter a question shown as below:

      1>Linux version:  L5.10.72-2.2.2

      2>We do as 《i.MX DSP User's Guide》chapter 4.3, but uart4 can't output the log message.

          Only in kernel, we can output the log message from uart4, the harware is ok.

     

       Can you help to check and fix it?

       Thanks very much.

----log screen shot.

jimmyli_0-1683169176524.png

 

Labels (1)
0 Kudos
Reply
4 Replies

2,127 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @jimmyli,

I hope you are doing well.

UART4 is used for Cortex-M7 core.
Disable UART4 in Linux OS & M7 core as DSP firmware runs on HiFi core.
In ATF, UART4 should be allocated to hifi4 core using RDC. 

Thanks & Regards,
Sanket Parekh
0 Kudos
Reply

2,123 Views
jimmyli
Contributor V

Hi Dhruvit,

     Got it.

      Thanks very much.

0 Kudos
Reply

2,057 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @jimmyli 

I hope you are doing well.

I'm glad to help you, if the issue is solved, can I close the thread?

Thanks & Regards,

Sanket Parekh

0 Kudos
Reply

2,022 Views
jimmyli
Contributor V

Hi Sanket,

       Sorry for replying too late.

       Yes, we have resolve the problem.

 

      Thanks very much.

Tags (1)
0 Kudos
Reply