DSP can't ouput debug log on IMX8MP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DSP can't ouput debug log on IMX8MP

1,533件の閲覧回数
jimmyli
Contributor IV

Hi,

      We are trying to run HIFI4 dsp on IMX8MP, but encounter a question shown as below:

      1>Linux version:  L5.10.72-2.2.2

      2>We do as 《i.MX DSP User's Guide》chapter 4.3, but uart4 can't output the log message.

          Only in kernel, we can output the log message from uart4, the harware is ok.

     

       Can you help to check and fix it?

       Thanks very much.

----log screen shot.

jimmyli_0-1683169176524.png

 

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

1,478件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @jimmyli,

I hope you are doing well.

UART4 is used for Cortex-M7 core.
Disable UART4 in Linux OS & M7 core as DSP firmware runs on HiFi core.
In ATF, UART4 should be allocated to hifi4 core using RDC. 

Thanks & Regards,
Sanket Parekh
0 件の賞賛
返信

1,474件の閲覧回数
jimmyli
Contributor IV

Hi Dhruvit,

     Got it.

      Thanks very much.

0 件の賞賛
返信

1,408件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @jimmyli 

I hope you are doing well.

I'm glad to help you, if the issue is solved, can I close the thread?

Thanks & Regards,

Sanket Parekh

0 件の賞賛
返信

1,373件の閲覧回数
jimmyli
Contributor IV

Hi Sanket,

       Sorry for replying too late.

       Yes, we have resolve the problem.

 

      Thanks very much.

タグ(1)
0 件の賞賛
返信