DRDY polarity

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

DRDY polarity

跳至解决方案
2,404 次查看
wushengyong
Contributor II

The TFT uses DRDY signal, no HSYNC and VSYNC. The polarity of DRDY of TFT requires high active, but in iMX DS, it is active low, could the polarity to be set to high? the same question for CLK.

标签 (2)
1 解答
2,302 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  It is possible change the polarity of the IPU output. Please refer to IPUx_DI0_POL register

description in I.MX6 RM. Note, for i.MX6, signal IPUx_DIx_PIN15 is used DRDY/DV (Data
validation/blank, data enable
).


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
2,302 次查看
wushengyong
Contributor II

Got it, thanks!

0 项奖励
回复
2,303 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  It is possible change the polarity of the IPU output. Please refer to IPUx_DI0_POL register

description in I.MX6 RM. Note, for i.MX6, signal IPUx_DIx_PIN15 is used DRDY/DV (Data
validation/blank, data enable
).


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------