DRAM SDCKE external pull down resistors

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DRAM SDCKE external pull down resistors

Jump to solution
4,106 Views
atillametetured
Contributor V

Hi,

Sabre SD has them but HW guide states they are no longer needed because they have on-chip pull downs. I did not implement these in my design but it gets me wondering why it says "no longer". Was this fixed with a new series of chips, if so, how do I know I get the new ones? Do pull downs need to be activated or are they active by default?

I am using iMx6Q with T topology 4xDDR3L chips total of 16Gb and only the DRAM_SDCKE0.

Regards,

Mete

Labels (2)
1 Solution
3,734 Views
art
NXP Employee
NXP Employee

In case of DDR3/DDR3L memory, the SDCKE pull-downs are not required at all. They only might be required in case of LPDDR2 memory.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

6 Replies
3,734 Views
Yuri
NXP Employee
NXP Employee

Hello,

   More details why for DDR3: SDCKE[1:0] pull-down is used in the SDP\B,  although it is not recommended:
“DRAM_SDCKE0 and DRAM_SDCKE1 require external resistors (such as 10 kΩ) to GND to minimize current
drain during deep sleep mode (DSM). 
The BSP (Board Support Package) uses a common DDR routine for both fly-by and T-topology designs.
 Fly-by designs have parallel resistor termination on address lines, while T-topology does not.

During low-power self refresh, the BSP programs pad control register GRP_CTLDS to 0x00000000. Therefore,
DRAM_SDCKE0, DRAM_SDCKE1, and other associated GRP_CTLDS I/O are forced to the high-impedance state.

Because DRAM_SDCKE0 and DRAM_SDCKE1 are forced to high-Z, external pull-down resistors are required to
avoid floating outputs during standby. In Freescale designs, 10 kohm resistors are utilized for this purpose.
Any other termination on the DRAM_SDCKE0 and DRAM_SDCKE1 lines (such as 50 ohms) should not be present;
simulation should be performed to ensure CKE signal integrity.”

Regards,

Yuri.

0 Kudos
Reply
3,734 Views
atillametetured
Contributor V

Hello Yuri,

I found that in mx6q_4x_mt41j128.cfg 0x020e078c is set to 0x00000030 which impiles 40 Ohm DSE for Control signals. Where exactly is it set to 0x00000000? Is it in the linux bsp? Do you think it will be an issue for us where PD resistors are not included? How can we fix this if it is an issue?

Regards,

Mete

0 Kudos
Reply
3,734 Views
Yuri
NXP Employee
NXP Employee

Hello,

   Yes, Linux BSP during deep sleep mode (DSM) reconfigure the pad
control register in order to minimize current drain. No problems expected

when DSM is not used.

Regards,

Yuri.

3,734 Views
atillametetured
Contributor V

Hi Yuri,

Your help is appreciated.

Cheers,

Mete

0 Kudos
Reply
3,735 Views
art
NXP Employee
NXP Employee

In case of DDR3/DDR3L memory, the SDCKE pull-downs are not required at all. They only might be required in case of LPDDR2 memory.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,734 Views
atillametetured
Contributor V

Hi Artur,

Thank you very much.

Regards,

Mete

0 Kudos
Reply