DRAM Contoroller Optimization and Pattern Simulation for DDR3 and EMMC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DRAM Contoroller Optimization and Pattern Simulation for DDR3 and EMMC

1,402 Views
asou_junichi
Contributor I

Hi,

We are currently using i.MX6 Dual. 

But if i.MX6 Dual is replaced with i.MX6 Quad on the same PCB, is DRAM Controller Optimization needed to re-generate again for i.MX6 Quad?

Or can we re-use the one of i.MX6 Dual against the one of i.MX6 Quad?

BR,

JA

Labels (2)
0 Kudos
Reply
1 Reply

1,327 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello JA,

If the only change on the PCB is the swap from i.MX6D to the i.MX6Q, you may use the optimization you already have. However, it’s always a practice to perform some stress tests to make sure there are no other variables like manufacturing variations involved as well.

I hope this helps!

Regards,

0 Kudos
Reply