DOES yocto REALLY have iMX5 hardware support??

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DOES yocto REALLY have iMX5 hardware support??

984 Views
kemilewis
Contributor I

DOES yocto  REALLY have iMX5 hardware support??  According to their documentation. It does have gstreamer-1.0 support, but it is software decode only. Is this still true/documentation is accurate? Need gstreamer-1.0 support drivers for the chip level media processors for VPU - H/W decoder, and the IPU and DP - frame buffer and display interface.

0 Kudos
Reply
1 Reply

829 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Kemi,

      The final version of linux BSP for i.MX5 serials SoC should be L3.0.35 released together with LTIB(Linux Target Image Builder). You can also see source code for i.MX5 SoC in Yocto , but these source code for i.MX5 was not tested. So if you want to use source code for i.mx5 in Yocto, you will have to do more work on test or debug.

Have a nice day!

TIC weidong sun

0 Kudos
Reply