DMIC input volume very low

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DMIC input volume very low

1,437 Views
anushan
Contributor III

Hello Everyone,

I am trying to record voice through the dmic present on my board, the audio codec used is wm8962, the codec provides 1.8v to the dmic and dmic clock runs at 2.8MHz. But, when I record anything through the dmic i am not able to hear anything in the playback.

Kindly help to find a solution.

Regards,

Anusha

0 Kudos
Reply
1 Reply

1,381 Views
igorpadykov
NXP Employee
NXP Employee

Hi Anusha

one can try to tweak "attenuation" factor described in Table 7-7. Audio Mixer controls 

Linux Manual in Linux 5.4.3_1.0.0 Documentation

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply