DMA usage of gstreamer when using vpuenc_h264 Hardware Encoder in imx8mp

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DMA usage of gstreamer when using vpuenc_h264 Hardware Encoder in imx8mp

1,018 Views
karthicknarayanan
Contributor I

We are using following gstreamer pipeline for recording video using IMX8MPLUS 

gst-launch-1.0 -e v4l2src device=/dev/video2 ! video/x-raw,width=640,height=480 ! clockoverlay time-format="%D %H:%M %S" halignment=right valignment=bottom shaded-background=true font-desc="Sans,12" ! vpuenc_h264 bitrate=5500 ! h264parse ! mp4mux ! filesink location=test.mp4

we are using this pipeline as it consumes less CPU and power.

We need to record video using DMA so I have edited the pipeline

gst-launch-1.0 -e v4l2src device=/dev/video2 io-mode=dmabuf ! video/x-raw,width=640,height=480 ! clockoverlay time-format="%D %H:%M %S" halignment=right valignment=bottom shaded-background=true font-desc="Sans,12" ! vpuenc_h264 bitrate=5500 ! h264parse ! mp4mux ! filesink location=test.mp4

It was working fine but I cannot find any difference in CPU usage and power consumption between two pipelines.

Is there any methods to check that the video is actually getting recorded using the DMA?

Is vpuenc_h264 uses DMA by default in gstreamer ?

Do DMA play the role for lesser CPU usage ? 

0 Kudos
Reply
1 Reply