DMA-BUF sync not working and "causing issues" in newer 5.10 / 5.15 kernels?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DMA-BUF sync not working and "causing issues" in newer 5.10 / 5.15 kernels?

1,308件の閲覧回数
crg7475
Contributor III

This commit from NXP's gst-plugins-base fork states that DMA_BUF_IOCTL_SYNC should not be used because "it causes issue".

https://source.codeaurora.org/external/imx/gst-plugins-base/commit/?h=MM_04.06.04_2112_L5.15.y&id=6d...

Which issue is that? I can see that the DMA_BUF_IOCTL_PHYS is necessary to actually sync the CPU cache with the DRAM (which is what DMA_BUF_IOCTL_SYNC should do, but it's broken in the NXP kernel). But what issues does the broken DMA_BUF_IOCTL_SYNC cause?

Furthermore, will this be resolved? Is this planned?

0 件の賞賛
返信
0 返答(返信)