DHCP issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DHCP issue

1,032件の閲覧回数
reghund1985
Contributor I

HI ,

i was using MIMRT1024 with dhcp mode and connected multiple devices in the same netwrok with different mac id . some period device is getting some error (releasing token twice). I was using Cortex M3 ethernet driver (Iam not sure whether am using latest driver or not) . Can any one help me to give some idea on the issue / any link to get the latest driver lib

 

Thanks 

Reghu

0 件の賞賛
返信
1 返信

1,008件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @reghund1985 ,

   If you are using the RT1024, I highly recommend you use the RT1024 SDK which can be downloaded from this link:

https://mcuxpresso.nxp.com/en/builder?hw=MIMXRT1024-EVK

   SDK_2_13_0_MIMXRT1024-EVK\boards\evkmimxrt1024\lwip_examples\lwip_dhcp

   Don't use the Cortex M3 driver, use the RT1024 driver.

 

Wish it helps you!

If you still have questions about it, please kindly let me know.

Best Regards,

Kerry

0 件の賞賛
返信