DFI FS700-M60 and YOCTO Project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DFI FS700-M60 and YOCTO Project

2,226 Views
giovannifalcata
Contributor I

Does someone know if there is a Yocto's project layer available (and the BSP) for this family of boards?

Thanks. Giovanni

Labels (2)
0 Kudos
Reply
3 Replies

2,043 Views
igorpadykov
NXP Employee
NXP Employee

Hi Giovanni

seems this board is supported, one can look at

https://github.com/torvalds/linux/blob/master/arch/arm/boot/dts/imx6qdl-dfi-fs700-m60.dtsi

http://lxr.free-electrons.com/source/arch/arm/boot/dts/imx6dl-dfi-fs700-m60.dts

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,043 Views
giovannifalcata
Contributor I

Hi Igorpaddykov,

Thanks for the links, but there I do not see any references to the Yocto project. Those seem to be a generic implementations of Linux on this hw platform. What do you think about?

Guido

0 Kudos
Reply

2,043 Views
igorpadykov
NXP Employee
NXP Employee

Hi Giovanni

suggest to post this to to meta-fsl-arm mailing list, so that someone

familiar with this board could try to assist you.

https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards

igor

0 Kudos
Reply