DEBUGGING CORTEX M4 OF SOLOX!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DEBUGGING CORTEX M4 OF SOLOX!

2,476件の閲覧回数
soumyasatheesh
Contributor II

I am trying to debug only cortex m4 on which mqx sample application is running.I using the IAR embedded workbench 7.4 version and an IAR I-jet.What are the configurations need to be done?I meant about the .ddf files and  setup macro files?The IAR version already has a probe config file for imx6solox which i had included.Where are the links for the setup macro file and .ddf files?Please guide me with this issue.

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,212件の閲覧回数
soumyasatheesh
Contributor II

Hi,

the link you mentioned is about Jlink,but i am using  IAR I-jet.I am able to pause and resume the application but not able to set the breakpoints.I did not get the setup macro and ddf files.

0 件の賞賛
返信

2,212件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

right, mentioned link is about Jlink but customers used it with

IAR, suggest to post there about additional details.

~igor

0 件の賞賛
返信

2,212件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Soumya

please check below links

I.MX6SX SoloX Debugging 

[SOLVED] Freescale IMX6SoloX support - J-Link/Flasher related - SEGGER Forum 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信