DDR3 sabrelite

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,395件の閲覧回数
douglasbolton
Contributor III

The current DDR3 dram (MT41J128M16HA-15E) on the sabrelite reference board has an end of life notice from Micron. They are recommending MT41K128M16JT-125:K a 1.35 volt part that is backwards compatible with 1.5 volt systems.

What DDR3 replacement are Freescale going to use on their Sabrelite reference boards ?

Thanks

Doug.

 

ラベル(1)
0 件の賞賛
返信
1 解決策
2,112件の閲覧回数
Yuri
NXP Employee
NXP Employee

From Mark Middleton:

We are putting the Micron MT41K128M16JT part on the SABRE Smart Device board and the Micron MT41K256M16JT part on the SABRE AI board.

We were basically forced to do that because Micron went EOL on their 1.5V part.

The interesting news is that, while we are still using 1.5V rails for the new part, the customer can easily change the voltage rail to 1.35V at boot time, before the DDR3 is loaded, and then give it a test try. Might have to tweak on some register settings a bit to make sure everything is okay, but should not be a huge effort. Officially, we are not going to test that all out. Not enough resources.

Samsung devices: They should work, but we have not tested any. K4B2G1646E is the equivalent part to MT41K128M16JT

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,112件の閲覧回数
douglasbolton
Contributor III

Thank you Mark

0 件の賞賛
返信
2,113件の閲覧回数
Yuri
NXP Employee
NXP Employee

From Mark Middleton:

We are putting the Micron MT41K128M16JT part on the SABRE Smart Device board and the Micron MT41K256M16JT part on the SABRE AI board.

We were basically forced to do that because Micron went EOL on their 1.5V part.

The interesting news is that, while we are still using 1.5V rails for the new part, the customer can easily change the voltage rail to 1.35V at boot time, before the DDR3 is loaded, and then give it a test try. Might have to tweak on some register settings a bit to make sure everything is okay, but should not be a huge effort. Officially, we are not going to test that all out. Not enough resources.

Samsung devices: They should work, but we have not tested any. K4B2G1646E is the equivalent part to MT41K128M16JT

0 件の賞賛
返信