Suggestion for BT/Wifi/Apple identification chip

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Suggestion for BT/Wifi/Apple identification chip

Jump to solution
909 Views
shuntanaka-b356
NXP Employee
NXP Employee

Could someone advice suggested BT & Wifi module for IMX SABRE AI?

I see that the Bluetooth and Wi-Fi module are optional as well as the Apple identification chip for SABRE AI. Is it possible to buy also these optional directly from Freescale or need to go through distributor?

Labels (1)
0 Kudos
1 Solution
711 Views
igorpadykov
NXP Employee
NXP Employee

Hi Shun, one can use Atheros chips (for example AR6003 WiFi)

or Silex modules

141-00207-509C_iMX6X_SX-SDCAN_QSG.pdf

Regarding Apple I am not sure where did you find references to it.
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
712 Views
igorpadykov
NXP Employee
NXP Employee

Hi Shun, one can use Atheros chips (for example AR6003 WiFi)

or Silex modules

141-00207-509C_iMX6X_SX-SDCAN_QSG.pdf

Regarding Apple I am not sure where did you find references to it.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos