DDR3 Porting Problem on imx6ULL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR3 Porting Problem on imx6ULL

Jump to solution
4,430 Views
guochgz
Contributor III

hello,

       I am using SkHynix H5TC2G63GFR-PBI DDR3 on imx6ull, there is some question about DDR3 Porting, Is there someone can help me? thanks first. 

       Q1: Is there a special DDR3_Script_Aid tools for imx6ull? I have download a imx6ul aid that  the name is <I.MX6UL_DDR3_Script_Aid_V0.02.xlsx> from this community

https://community.nxp.com/docs/DOC-329899

. is this ok? 

       Q2: how to setup DDR3_Script_Aid? there are some item which I have no idea.

Device Information
Manufacturer:MicronSKhynix
Memory part number:MT41K256M16HA-125H5TC2G63GFR-PBI
Memory type:DDR3-1600DDR3-1600
DRAM density (Gb)42
DRAM Bus Width1616
Number of Banks88
Number of ROW Addresses1514
Number of COLUMN Addresses1010
Page Size (K)22
Self-Refresh Temperature (SRT)ExtendedExtended
CAS READ latency (CL)8?

Programmable CAS latency

6, 7, 8, 9, 10, 11, 12 and 13

supported

tRCD=tRP=CL (ns)13.75?
tRC Min (ns)48.7550.625
tRAS Min (ns)3537.5
System Information
i.Mx Parti.MX6ULiMX6ULL
Bus Width1616
Density per chip select (Gb)42
Number of Chip Selects used11
Total DRAM Density (Gb)42
DRAM Clock Freq (MHz)400400
DRAM Clock Cycle Time (ns)2.51.25?
Address Mirror (for CS1)DisableDisable
SI Configuration
DRAM DSE Setting - DQ/DQM (ohm)4848
DRAM DSE Setting - ADDR/CMD/CTL (ohm)4848
DRAM DSE Setting - CK (ohm)4848
DRAM DSE Setting - DQS (ohm)4848
System ODT Setting (ohm)6060

Q3: the last one about NXP DDR Test tool , What is the Value about MR1 Values(Hex)? 

pastedImage_3.png

Labels (1)
0 Kudos
Reply
1 Solution
4,152 Views
Yuri
NXP Employee
NXP Employee

Correct - 4.

~Yuri.

View solution in original post

0 Kudos
Reply
3 Replies
4,152 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  

   Customers can use the following tool:

 

“i.MX6ULL_DDR3_Script_Aid”

 

https://community.nxp.com/docs/DOC-333791

MR1 value should be the same as in the initialization script.

 

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos
Reply
4,152 Views
guochgz
Contributor III

Thanks Yuri.

"MR1 value should be the same as in the initialization script." What does this mean?  

I have found this in ddr stress tools dir. 

pastedImage_1.png

so MR1 Value should be 0004? 

0 Kudos
Reply
4,153 Views
Yuri
NXP Employee
NXP Employee

Correct - 4.

~Yuri.

0 Kudos
Reply