Hello,Pavel,
I have ever confirmed the similar question with HW dept, it is no problem to use low 32bit bus of i.mx6 memory interface.
In i.MX SoC , The clock source of CLK0 & CLK1 is the same. So you can use them like this:
(1) Using same clock for reading or writing one 32 bit .
CS0: D0~D31 ( 2 DDR3 ICs)
CLK0
CS1: D0~D31 (2 DDR3 ICs)
CLK1
(2) Every 16bit uses same clock.
CS0: D0~D15 (1 DDR3 IC)
CLK0
CS0: D16~D31 (1 DDR3 IC)
CLK1
CS1: D0~D15 (1 DDR3 IC)
CLK0
CS1: D16~D31 (1 DDR3 IC)
CLK1
The above mothod is for you as a reference.
Regards,
Weidong