DDR3 Bit Swaaping

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,722件の閲覧回数
muralikrishna
Contributor I

We swapped the DDR3 bits as recommended.

How to map these bits to processor while initializing.

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 解決策
3,539件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
3,540件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 件の賞賛
返信
3,539件の閲覧回数
art
NXP Employee
NXP Employee

Also, when swapping the byte lanes, don't forget to route correctly the strobe and mask signals, i.e. DQMx, DQSx and DQSx_B, corresponding to these byte lanes.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,539件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Murali

there is no need for additional mapping or software reconfiguration, as

it is done automatically. Bit swapping is described in sect.3.5.1 Swapping data lines IMX6DQ6SDLHDG also

below part of p.4 SPF-27392 Sabre Schematic i.MX6_SABRE_SDP_DESIGNFILES :

SPF-27392   p.4.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,539件の閲覧回数
muralikrishna
Contributor I

Hi igor,

Bit swapping in Hardware is taken care.

How to implement those bit swappings in software to write or read to DDR3

Murali

0 件の賞賛
返信
3,539件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Murali

in general it is not possible to implement bit swappings in software.

If you followed Freescale recommmendations, there is no need

for additional mapping or software reconfiguration,

Best regards

igor

0 件の賞賛
返信