E:\soloX\Broad Bring up\DDR test\Sol SoloX larger RAM\DDR_Stress_Tester_V1.0.3_ENCORE\Binary>DDR_Stress_Tester.exe -t mx6x -df scripts\my.txt
MX6SX opened.
HAB_TYPE: DEVELOP
Image loading...
download Image to IRAM OK
Re-open MX6x device.
Running DDR test..., press "ESC" key to exit.
******************************
DDR Stress Test (1.0.3) for MX6SX
Build: Jun 25 2014, 12:09:14
Freescale Semiconductor, Inc.
******************************
=======DDR configuration==========
DDR type is DDR3
Data width: 16, bank num: 8
Row size: 14, col size: 10
Chip select CSD0 is used
Density per chip select: 256MB
==================================
What ARM core speed would you like to run?
Type 0 for 650MHz, 1 for 800MHz, 2 for 1GHz
ARM set to 800MHz
Please select the DDR density per chip select (in bytes) on the board
Type 0 for 2GB; 1 for 1GB; 2 for 512MB; 3 for 256MB; 4 for 128MB; 5 for 64MB; 6
for 32MB
DDR density selected (MB): 256
Calibration will run at DDR frequency 400MHz. Type 'y' to continue.
If you want to run at other DDR frequency. Type 'n'
DDR Freq: 396 MHz
Would you like to run the write leveling calibration? (y/n)
You have chosen not to run the write level calibration
Would you like to run the DQS gating, read/write delay calibration? (y/n)
Starting DQS gating calibration...
. . . . . . . . . . . . . . ERROR FOUND, we can't get suitable value !!!!
dram test fails for all values.
The DDR stress test can run with an incrementing frequency or at a static freq
To run at a static freq, simply set the start freq and end freq to the same valu
e
Would you like to run the DDR Stress Test (y/n)?