DDR clk value

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DDR clk value

1,470 次查看
dhanunjay
Contributor III

HI All,

I want to change imx6 DL DDR clk frequency to 410MHz, is it possible? can you pl. give example bare-metal ?

Is it possible to change DDR clk frequency run time?

标签 (3)
0 项奖励
回复
1 回复

1,343 次查看
igorpadykov
NXP Employee
NXP Employee

Hi DHANUNJAY

it can be changed running code from iRAM for changing system PLL,

check sect.18.5.1.3.3 System PLL, sect.18.5.1.5.3 PLL clock change

i.MX6DQ Reference Manual: http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf.

In runtime the same procedure can be used. For example bare-metal please

create service request.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复