DDR Test Tool Can't Open USB device for IMX6ULL EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR Test Tool Can't Open USB device for IMX6ULL EVK

3,655 Views
tanly
Contributor I

Hi,

I could could not get the DDR Test Tool to connect to the USB Device. It is set to serial boot, and I can down uboot and linux using uuu.  However, DDR Test Tool kept giving me ERROR: Can't Open USB device. The following are the setting

* Connected to USB OTG

* Configure to Serial booting (I even verified that uuu can detect usb otg)

* Loaded init script EVK_IMX6ULL_DDR3L_400MHz_512MB_16bit_V1.2.inc

* Select TARGET: MX6ULL

I wonder if I missed any steps

Labels (1)
Tags (1)
0 Kudos
Reply
4 Replies

1,352 Views
hamzehnasajpour
Contributor II

I have ran it as admin, also as you can see its detected by uuu tools. but still the usb cant be openned by DDR Test Tool. Any idea?

Screenshot 2024-11-13 171710.png

0 Kudos
Reply

1,359 Views
hamzehnasajpour
Contributor II

I have the same issue with my imx6q custom board.

1. the boot mode is set to `01` Serial Downloader.

2. It's recognized by Windows and listed in the devices. I can see it in the list by uuu -lusb command.

3. I can send the uboot by uuu tool.

4. But when I am trying to run DDR stress test I get:

Can't Open USB device.

 

Any idea?

0 Kudos
Reply

3,553 Views
igorpadykov
NXP Employee
NXP Employee

Hi Tan

one can try on different PC, also please try first power-up

board then attach usb cable to computer. May be useful below presentation

showing usage ddr test step by step

https://community.nxp.com/docs/DOC-331528 

i.MX 6/7 DDR Stress Test Tool  

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,553 Views
tanly
Contributor I

Hi Igor,

Thanks for quick reply. 

Actually, I found a problem on one of my machines.  I did try on a desktop PC and a laptop, both didn't not work.  However, I found the virtualbox that I use for debugging uboot using the USB-OTG debugging for IMX, seems rename the usb drive in windows to virtualUSB, and DDR Test Tool does not seems to like it.  When VirtualBox was closed, DDR Test Tool was able to detect USB.

However, I still don't know what was wrong on my PC, but probably something similar or driver related.

Tan

0 Kudos
Reply