DDR Porting Issue on MX6DL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR Porting Issue on MX6DL

1,356 Views
tony_l_cai
Contributor III

Hi,all

     On our board(MX6DL) we ported DDR on Android 5.0, and the board can not install APK,when installing, it will crash. But the same porting copy on Android 4.2, all is perfect. So Could you give me some explaination? Could I contact with FSL DDR RD to talk about this complicated problem? Could you give me the password about the porting xls? I need to know how my DDR parameters transition to DDR porting copy. And when encountered this problem, how to regulate my DDR porting?

Labels (4)
0 Kudos
Reply
1 Reply

1,233 Views
igorpadykov
NXP Employee
NXP Employee

Hi Tony

you can try to run Linux with new ddr, to know if APK issue

is related to ddr. Below resources devoted to porting new DDR :

i.MX6/7 DDR Stress Test Tool V2.40

i.MX6 DDR Stress Test Tool V1.0.3

https://community.freescale.com/docs/DOC-101708

In general you can elevate your requirements contacting local fae

and NXP Professional Services:

http://www.nxp.com/pages/freescale-professional-services:PROFESSIONAL-SERVICES

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply