DDR Configurations

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR Configurations

1,903 Views
ailtonlopes
Contributor III

I’m having some problems with the DDR when executing the code specially after configuring the EPIT driver the memcpy stop working, and when for example I use the secure monitor to go from ns to secure the code crash when doing the “movs lr” where lr has the address of a guest OS, so I wanted to ask what is the correct configuration of the DDR on the IMX6quad board.

kind regards 

Ailton Lopes

Labels (1)
1 Reply

1,634 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  use the following

DRAM Customization on i.MX6x 

 

As for memory tools:

https://community.nxp.com/docs/DOC-236354 

It makes sense to check memory:

i.MX6/7 DDR Stress Test Tool V2.80 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!