DDR Address in iMX8M Mini

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR Address in iMX8M Mini

1,550 Views
borisberman
Contributor III

Hello,

We'd like to get addressed to more that 3G-RAM.

IMX8MMRM - claims that:
1_0000_0000 2_3FFF_FFFF DDR Address 5120MB DDR Memory (Quad-A53 only)
  4000_0000 FFFF_FFFF DDR Address 3072MB DDR Memory (All modules)

The official NXP U-boot repository does not have any examples that show how to configure CONFIG_SYS_SDRAM_BASE=0x100000000
https://source.codeaurora.org/external/imx/uboot-imx.git

We'd appreciate it if you could help us in configuring this correctly.

Best Regards,

Boris

Labels (1)
0 Kudos
Reply
1 Reply

1,398 Views
igorpadykov
NXP Employee
NXP Employee

Hi Boris

config files were sent via mail.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply