DCD Table for i.MX6 Dual Plus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DCD Table for i.MX6 Dual Plus

2,115件の閲覧回数
rdattilio
Contributor II

Hi:

Can someone point me to the DCD Table values to use with an MX6 Dual Plus?

Regards

Robert

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,720件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

DCD table is board dependent, so you should adapt it according to the DDR memory you have in your board.

Here is an example for the mx6sabreauto board based on a quad plus:

uboot-imx.git - Freescale i.MX u-boot Tree

Regards,

Fabio Estevam

0 件の賞賛
返信

1,720件の閲覧回数
rdattilio
Contributor II

Related question: if you have an existing board running with an i.MX6 Quad processor and then you go upgrade the processor to the Quad Plus version, do you have to make any changes to the DCD entries that are applied/loaded by the bootloader to adjust for the change in the processor?

0 件の賞賛
返信