DATAIO image creation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DATAIO image creation

3,865件の閲覧回数
jacklu
Contributor II

Hi,

In IMX6SL platform, is DATAIO image supported? We want to do the EMMC download before factory SMT.

Thanks!

ラベル(2)
タグ(1)
0 件の賞賛
返信
4 返答(返信)

3,703件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi jack

yes, one can write image to emmc before soldering it on board,

please refer to sect.4.3 Preparing an SD/MMC card to boot

attached document.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,703件の閲覧回数
jacklu
Contributor II

Dear Igorpadykov,

I really appreciate your help.

Our project is an android proj, so, this document is a little different from our requirement.

Could you help to release the method for DATAIO on android?

Thank You!

BRs,

Jack

0 件の賞賛
返信

3,703件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi jack

please refer to attached file sect.4.1.3 Downloading images with dd utility

Best regards

igor

3,703件の閲覧回数
jacklu
Contributor II

Hi Igorpadykov,

Thank you.

I will try it.

BRs,

Jack

0 件の賞賛
返信