Customized QuadSPI Look-up Table/Flash Access Scheme

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Customized QuadSPI Look-up Table/Flash Access Scheme

873 Views
martinzohlhuber
Contributor I

Hello

i.MX 7Dual Applications Processor Reference Manual, Rev. 0.1, 08/2016

implies (Section Flash Devices) that a user can create customized QuadSPI Instruction with Look-up Table and Programmable Sequence Engine.

Figure 10-17. Serial Flash Access Scheme illustrates a pattern:

Instruction (1 Byte) – Address (3/4 Byte) – Mode  (1 Byte) – Dummy (max 64 Byte) – Data

My Quad-SPI Device expects scheme:

Instruction (1 Byte) – Address (4 Byte) – Value (2+ Byte) – Dummy (max 16) – Data

With “Value” are two byte sent from i.MX to the device (like length of the data to be read/written)

Is it possible to define such a scheme?

How should the Look-Up Table be defined?

CMD   | 0xAB

ADDR  | 0x20

???? | 0x0004

DUMMY | 0x0A

READ  | 0x04

STOP  | 0x00

Thanks

Martin

Labels (1)
Tags (3)
0 Kudos
Reply
1 Reply

754 Views
igorpadykov
NXP Employee
NXP Employee

Hi Martin

yes such sequence can be defined, please look at examples in

sect.10.2.8.1 Example Sequences i.MX7D Reference Manual

http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7DRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply