Custom board struck at loading Uboot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Custom board struck at loading Uboot

跳至解决方案
1,650 次查看
pratyushtomar
Contributor IV

We have made a customised board based on imxulevk. We are using imx6ul procesor(IMX6UL G0) and lpddr2 ram (2Gb, Actual part is of 4Gb size with 32 bit data but only lower 16 bits are in use) and eMMC (4 GB). Thus we are using Mfg tool for downloading image but Mfg tool strucks at loading UBoot step with no error message. We have attached the dts file we are using and Mfg tool log. Can anyone please point where we may be making mistake?

Original Attachment has been moved to: MFG.log.zip

Original Attachment has been moved to: ucl2.xml.zip

Original Attachment has been moved to: imx6ul-14x14-evk.dts.zip

标签 (3)
0 项奖励
回复
1 解答
1,469 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Pratyush

for new board/ddr mfg tools firmware should be rebuilt,

please refer to sect.6.2 Manufacturing Tool, MFGTool attached

Yocto Guide. Please run ddr test and find new calibration settings

(enter them in uboot *.cfg file). Also remove for G0 unused modules in

linux build configs.

https://community.freescale.com/docs/DOC-105652 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,470 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Pratyush

for new board/ddr mfg tools firmware should be rebuilt,

please refer to sect.6.2 Manufacturing Tool, MFGTool attached

Yocto Guide. Please run ddr test and find new calibration settings

(enter them in uboot *.cfg file). Also remove for G0 unused modules in

linux build configs.

https://community.freescale.com/docs/DOC-105652 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------