Custom board MFG tool support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Custom board MFG tool support

2,412 Views
vijaikumar
Contributor III

Hi All,

         We are trying to add support for MFG tool in our board. But MFGtool hangs on loading our custom uboot. It is stuck at loading uboot. How can it be resolved?

0 Kudos
Reply
3 Replies

1,935 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vijai

Mfg toos firmware should be rebuilt with new ddr settings for custom board

(located in uboot dcd header), they can be found from DDR test results

https://community.freescale.com/docs/DOC-96412

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,936 Views
vijaikumar
Contributor III

Hi ,

                          I have built custom firmware (uboot kernel and initramfs). But when trying to load it with MFG Tool it hangs at "Loading uBoot". It successfully loads the SABRESD uboot but not mine.

0 Kudos
Reply

1,936 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vijai

could you provide full log ? You can try to rename custom uboot to name

which is used by "SABRESD uboot" (which loads succesfully, as you mentioned)

Best regards

igor

0 Kudos
Reply