Custom IMX6Q Hardware Board Bringup Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Custom IMX6Q Hardware Board Bringup Issue

1,700件の閲覧回数
rajniks
Contributor I

Hello,

I have a custom IMX6Q based hardware. I have checked the power supplies and sequencing of these power supplies and that seems to be okay. I have measured various CAP voltages and they are also fine except VDDUSB_CAP which is 2.7V instead of 3V. Is this a problem?

I have been trying to boot in Serial downloader mode by setting the boot mode pins as required but the Host machine doesn't detect my  board as HID complaint device as explained in DDR Tester User manual.

Can someone suggest some ways in order to make sure that the USB OTG Serial downloader works. Any suggestion is welcome.

Thanks & Regards

Raj Nikumbh

ラベル(2)
0 件の賞賛
返信
1 返信

1,497件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Raj

you can try to test processor with SDK (one can run it with jtag)

and test USB interface

i.MX 6Series Platform SDK : Bare-metal SDK

and check all items given in Chapter 2 Design Checklist

Chapter 8 Avoiding Board Bring-up Problems

IMX6DQ6SDLHDG  IMX6DQ6SDLHDG, Hardware Development Guide

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信