Current leakage on i.MX7D before power on sequence

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Current leakage on i.MX7D before power on sequence

1,139件の閲覧回数
brucetsai
NXP Employee
NXP Employee

The customer system is dual board design.

A board is Other brand CPU+OSC

B board is i.MX7D+XTAL

They shared A board's OSC clock channel to i.MX7D external clock input.

 The configuration in kernel: SD1_DATA1 => CCM_EXT_CLK2

1.jpg

But the power time slot of A board is earlier than B board.

So SD1_DATA1 has clock input from A board OSC before i.MX7D start its power on sequence.

It causes current leakage into the other two pins(NVCC_SD1 & VLDO3_3V3).

Signal of SD1_DATA1 (Red)

Signal of NVCC_SD1(Blue)

Signal of VLDO3_3V3(Green)

2.jpg

The customer would like to know what is the side effect under this condition.

By the way,we get information from i.MX6 datasheet about current leakage of power on sequence.

pastedImage_4.png

But we can't catch any information like this on i.MX7D datasheet.

Is there any version difference on it?

ラベル(1)
0 件の賞賛
返信
1 返信

973件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   Section 4.1.11 (Power supplies usage) of the i.MX7 Datasheet (IMX7DCEC,
Rev. 5, 07/2017) states: "I/O pins should not be externally driven while the I/O
power supply for the pin (NVCC_xxx) is OFF. This can cause internal latch-up
and malfunctions due to reverse current flows."


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信