Current Issue : High current value after poweroff

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Current Issue : High current value after poweroff

2,740件の閲覧回数
snan1z
Contributor I

Hi,

 

I'm dealing with an i.mx28 project whose products will enter standby mode if power is down and in the standby mode it will use battery(3.6V, 400mA). But in the standby mode(after poweroff command), it spents 60mA and it is so high for us.

 

How can i decrease spent current in the standby mode ?

 

Thanks for any help.

 

Best Regards,

Sinan

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,524件の閲覧回数
chrdcv
Contributor II

Hello!

You can check my post: IMX287 Power Supply Issues

Maybe the answer of your question too.

BR,

Christian

0 件の賞賛
返信

2,524件の閲覧回数
snan1z
Contributor I
Sorry for mistake, it is 400mA/h
0 件の賞賛
返信

2,524件の閲覧回数
chrdcv
Contributor II

Hello snan snan! I'm faced the same trouble! Anyone can help-me?

0 件の賞賛
返信