Cross compilation with alsa

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Cross compilation with alsa

1,966 次查看
claudiaalvarado
Contributor I

Hello!  I have a general question.  We are cross compiling on a Linux machine for an ARM processor on an embedded device.  When compiling, we specify paths for the include files and our cross compiled Alsa library.  We then try to port this to our embedded device(iMX6UL).  When trying to run the executable on the embedded device we get two problems:

  1. it doesn’t recognize the PCM device called ‘default’— I think we just need to call this out with hw:0,0 but we need to play with this.
  2. We get this error: “ALSA lib conf.c(snd_config_update_r)Cannot access file /path/to/alsa.conf"
    1. The path that it lists is the path to our cross compiled alsa lib on our linux box… so it seems that in the compilation process, this path is preserved and transferred to the executable somehow.

So my question is, is there a way to specify two different library paths for the two devices (linux and embedded) while compiling so that when we port to the embedded device, the executable knows where to look for the alsa library?  Normally, this wouldn’t be an issue because the default on a linux machine is usr/include, which I believe gets searched by default (?).  However, on our embedded device, the path is different.

Thanks in advance!

标签 (4)
标记 (2)
0 项奖励
回复
2 回复数

1,427 次查看
purvi_billore1
Contributor III

How did you cross compiled alsa-library and alsa-utils for iMX6?

0 项奖励
回复

1,427 次查看
jimmychan
NXP TechSupport
NXP TechSupport

are you using Yocto?

0 项奖励
回复