Creating own recipe in yocto

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Creating own recipe in yocto

ソリューションへジャンプ
2,396件の閲覧回数
manjunathjoshi
Contributor V

Hello all,

Is there any way that we can create a recipe which can simply copy a file from host computer to the bitbake process so that after the complete bitbake process we may just have the file in the right place in yocto filesystem?

I know this is weird but is there a way? I tried as shown below it didn't work. do_install failure.

this is the .bb file in a new layer i have created.

SUMMARY = "Example to copy from my filesystem to yocto filesystem"

DESCRIPTION = "Not needed"

SECTION = "examples"

LICENSE = "MIT"

LIC_FILES_CHKSUM += "file://README;md5=0d20a0079cbd6add839dcca5f80c7d0b"

PR = "r0"

DEPENDS = "boost"

SRC_URI="file://README \

        "

S="${WORKDIR}"

do_install() {

     install -m 0755 ${WORKDIR}/README  ${D}$/usr/sbin/README

}

Regards,

Manju

ラベル(3)
0 件の賞賛
返信
1 解決策
1,745件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Manju,

Your recipe looks good in general but it may need some tweaking. Would you please try with the following changes? (The first part of the recipe looks good).

do_install() {

   install -d  ${D}$/usr/sbin/

     install -m 0755 ${WORKDIR}/README  ${D}$/usr/sbin/

}

FILES_${PN} = "$/usr/sbin/README"

I hope this helps, let us know of your progress! One would think that copying a file into the filesystem should be pretty straightforward but it’s not so trivial in Yocto. I’m sure other community users may have the same question.

Regards,

Gus

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,746件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Manju,

Your recipe looks good in general but it may need some tweaking. Would you please try with the following changes? (The first part of the recipe looks good).

do_install() {

   install -d  ${D}$/usr/sbin/

     install -m 0755 ${WORKDIR}/README  ${D}$/usr/sbin/

}

FILES_${PN} = "$/usr/sbin/README"

I hope this helps, let us know of your progress! One would think that copying a file into the filesystem should be pretty straightforward but it’s not so trivial in Yocto. I’m sure other community users may have the same question.

Regards,

Gus

0 件の賞賛
返信
1,745件の閲覧回数
manjunathjoshi
Contributor V

Hello gusarambula,

I am sorry i didn't update this on the community. Your answer is right i have already done this. But right now i am in to writing a recipe which does every bit of a standard one. I have posted the same in

Custom recipe for YOCTO

Please reply if you have needed information on the same.

Thanks a lot in advance.

Regards

Manju

0 件の賞賛
返信