Creating file in file system reg

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Creating file in file system reg

885 Views
sachusanal
Contributor III

hai ,

I need to create one file which contains kernel version in file system.It will create automatically when the kernel build occured

Labels (1)
0 Kudos
Reply
1 Reply

820 Views
bpe
NXP Employee
NXP Employee

Execute this once the target is up:

cat /proc/version > running_kernel_version.txt


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply