Creating file in file system reg

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Creating file in file system reg

1,339件の閲覧回数
sachusanal
Contributor III

hai ,

I need to create one file which contains kernel version in file system.It will create automatically when the kernel build occured

ラベル(1)
0 件の賞賛
返信
1 返信

1,274件の閲覧回数
bpe
NXP Employee
NXP Employee

Execute this once the target is up:

cat /proc/version > running_kernel_version.txt


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信