Creating an extra framebuffer for imx6UL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Creating an extra framebuffer for imx6UL

1,561 Views
zc_tee
Contributor III

Hi all,

Is it possible to create an extra framebuffer for imx6UL. I need two framebuffers (/dev/fb0 and /dev/fb1) to be associate with the LCDIF interface of imx6UL.

Thank you.

Regards,

Tee

Labels (3)
0 Kudos
Reply
1 Reply

1,315 Views
igorpadykov
NXP Employee
NXP Employee

Hi ZC

please check linux documentation related to framebuffer

http://www.tldp.org/HOWTO/text/Framebuffer-HOWTO 

How can I add an additional framebuffer device in Linux? - Unix & Linux Stack Exchange 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply