Creating a bootable image

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Creating a bootable image

2,194 次查看
ken1_saito
Contributor I

I am following the document i.MX8 Boot process and creating a bootable image to create a bootable image for  MCIMX8M-EVK. I think I already have all I need to create one, but I am not sure which SCFW is suitable for my purpose because there are several variants in imx-sc-firmware.1.2 without any descriptions.

Selection_441.png

Could anyone tell me which one I should use?

Then I guess I also need  to rename it to scfw_tcm.bin to make the image. Is that correct procedure?

标签 (1)
0 项奖励
回复
2 回复数

2,078 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi Ken,

If you are using a MCIMX8M-EVK board, it includes a i.MX8M processor (4x Cortex-A53), which does not have the SCU (so, no SCFW is required).

The SCU-SCFW is for i.MX8QM (2x Cortex-A72 + 4x Cortex-A53) and i.MX8X (4x Cortex-A35) processors  and their MEK boards.


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------

2,078 次查看
ken1_saito
Contributor I

Hi Carlos,

Thanks for your help. Yes, you are right. I thought "Q" in i.MX8QM stands for Quad. Now I understand they are totally different.

Thanks,

Ken 

0 项奖励
回复