Create a dmabuf with libgbm

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Create a dmabuf with libgbm

2,539件の閲覧回数
jkmi
Contributor I

Hello,

I'm using iMX8 mini and trying to figure out if it's possible to create dumb buffers via libgbm on that board.

I want to achieve the following - 

1) open drm render node (not available on my board with vivante graphics. any ideas how to enable that?)

2) create gbm device

3) create gbm_bo

4) export handle

5) create image khr.

 

Is it possible to achieve that on imx8 provided it doesn't have drm render nodes?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,534件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello jkmi,

 

The i.mx8 does not provide renders node.and vivante is in binary form I don´t think it should be able to modify.

 

Regards

 

0 件の賞賛
返信

2,444件の閲覧回数
marcus-castlepeakinc
Contributor III

So is it possible to use drm on i.MX8 Plus?

0 件の賞賛
返信