Create Bootstream from Linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Create Bootstream from Linux

2,526件の閲覧回数
markusvalentin
Contributor II

Hi,

i have a custom compiled Linux and i want to encrypt and sign it. I have some questions:

1. Do i need to use Bootlets or can i get an ivt without them?

2. Is there any example .bd file?

kind regards

Markus

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 返信

2,296件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Markus

1. attached Linux Guide p.1-1 shows bootlet definition

2.  can be found in elftosb documentation

IMX_ELFTOSB_TOOL

Snippets, Boot Code, Headers, Monitors, etc. (4)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信