Could i.MX6SoloLite support MAX77696?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Could i.MX6SoloLite support MAX77696?

1,148 次查看
chihwenlee
Contributor II

refer to http://2014ftf.ccidnet.com/pdf/0058.pdf

There is Maxim MAX77696

but I can only find the drivers at kernel of kindle released by amazon (Kindle_src_5.6.2.1_2634390002.tar.gz)

标签 (1)
0 项奖励
回复
1 回复

724 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Chin

seems yes, as it is used on Warp board:

http://www.warpboard.org/wp-content/uploads/2014/01/WaRP_Mainboard_v1-12_Schematics-FSL.pdf

Technical Features | WaRPboard.org

for drivers one can look at:

https://github.com/Freescale/meta-fsl-arm-extra/blob/master/conf/machine/imx6sl-warp.conf#L40

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复