Hello,
In i.MX 6Dual/6Quad Applications Processor Reference Manual (imx6dqrm.pdf )
I see the following -
12.3.2 Core configuration
Table 12-4. Cortex-A9 Core configuration
PRELOAD_ENGINE_PRESENT - No
Does that mean that no automatic cache preload functionality is available on imx6?
Does that mean that PLD assembly instruction could not be used to optimize memory reads?
Thanks.
Hi,
According to the RM, the Cortex lacks of the Preload Engine.
Regards,
Alejandro
Hi,
Sorry for the delay,
It seems that you may use them but I suggest you to take a look at the errata first:
www.freescale.com/files/32bit/doc/errata/IMX6DQCE.pdf
Regards,
Alejandro
Thanks!
Does that mean that I can't use PLD assembler command to pull the data I need for calculations into L2 ?