Cortex A9 Preload Engine is not implemented in iMX6?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cortex A9 Preload Engine is not implemented in iMX6?

2,603 Views
sergeydanilov
Contributor III

Hello,

In i.MX 6Dual/6Quad Applications Processor Reference Manual (imx6dqrm.pdf )

I see the following -

12.3.2 Core configuration

Table 12-4. Cortex-A9 Core configuration

PRELOAD_ENGINE_PRESENT - No


Does that mean that no automatic cache preload functionality is available on imx6?

Does that mean that PLD assembly instruction could not be used to optimize memory reads?

Thanks.

Labels (6)
0 Kudos
Reply
6 Replies

2,255 Views
sergeydanilov
Contributor III

Please?

0 Kudos
Reply

2,255 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

According to the RM, the Cortex lacks of the Preload Engine.

Regards,

Alejandro

0 Kudos
Reply

2,255 Views
sergeydanilov
Contributor III

bump

0 Kudos
Reply

2,255 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

Sorry for the delay,

It seems that you may use them but I suggest you to take a look at the errata first:

www.freescale.com/files/32bit/doc/errata/IMX6DQCE.pdf

Regards,

Alejandro

0 Kudos
Reply

2,255 Views
sergeydanilov
Contributor III

Please?

0 Kudos
Reply

2,255 Views
sergeydanilov
Contributor III

Thanks!

Does that mean that I can't use PLD assembler command to pull the data I need for calculations into L2 ?

0 Kudos
Reply