Cortex A9 Preload Engine is not implemented in iMX6?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Cortex A9 Preload Engine is not implemented in iMX6?

2,509 次查看
sergeydanilov
Contributor III

Hello,

In i.MX 6Dual/6Quad Applications Processor Reference Manual (imx6dqrm.pdf )

I see the following -

12.3.2 Core configuration

Table 12-4. Cortex-A9 Core configuration

PRELOAD_ENGINE_PRESENT - No


Does that mean that no automatic cache preload functionality is available on imx6?

Does that mean that PLD assembly instruction could not be used to optimize memory reads?

Thanks.

标签 (6)
0 项奖励
回复
6 回复数

2,161 次查看
sergeydanilov
Contributor III

Please?

0 项奖励
回复

2,161 次查看
alejandrolozan1
NXP Employee
NXP Employee

Hi,

According to the RM, the Cortex lacks of the Preload Engine.

Regards,

Alejandro

0 项奖励
回复

2,161 次查看
sergeydanilov
Contributor III

bump

0 项奖励
回复

2,161 次查看
alejandrolozan1
NXP Employee
NXP Employee

Hi,

Sorry for the delay,

It seems that you may use them but I suggest you to take a look at the errata first:

www.freescale.com/files/32bit/doc/errata/IMX6DQCE.pdf

Regards,

Alejandro

0 项奖励
回复

2,161 次查看
sergeydanilov
Contributor III

Please?

0 项奖励
回复

2,161 次查看
sergeydanilov
Contributor III

Thanks!

Does that mean that I can't use PLD assembler command to pull the data I need for calculations into L2 ?

0 项奖励
回复