Corrupt display when running vivante fb tutorials

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Corrupt display when running vivante fb tutorials

2,685件の閲覧回数
kishorebhadri
Contributor I

Build system: Yocto Poky ( https://github.com/Freescale/meta-fsl-arm)

Linux kernel: 3.10.17_r0

vivante binaries: gpu-viv-bin-mx6q-3.10.17-1.0.2-hfp

Display: 12" (1280x800) LVDS

Board: Custom (based on imx solo)

Vertical white lines interlaced with black and white image is been displayed on the LVDS Screen while running the sample tutorials. The snap of the LCD is attached for the reference. Terminating the tutorial gives the right resolution and the color.

Frame buffer is functioning normally.

mode "1280x800-60"

        # D: 71.098 MHz, H: 49.374 kHz, V: 59.993 Hz

        geometry 1280 800 1280 800 32

        timings 14065 40 40 10 3 80 10

        accel false

        rgba 8/16,8/8,8/0,0/0

endmode

Any help/hint which can help us resolve this issue would be appreciated.

ラベル(4)
0 件の賞賛
返信
2 返答(返信)

2,559件の閲覧回数
kishorebhadri
Contributor I

This problem was resolved by passing the correct boot arguments (bpp was corrected)

0 件の賞賛
返信

2,559件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Kishore,

Please provide the bootargs that fix your issue.

Thanks

0 件の賞賛
返信