hdmi 1080p60 pixel clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

hdmi 1080p60 pixel clock

3,882 Views
endl
Contributor II

Hello

I'm testing 1080p60 rendering on hdmi.

For 1080p60 the pixel clock must be set to 148.5MHz

From "iMX 6Series Plarform SDK v1.1.0" I found this code

   switch (pclk) {    // pixel clock

        case 74250000:

        case 148500000:

            //clk output from 540M PFD1 of PLL3 

            HW_CCM_CHSCCDR.B.IPU1_DI0_CLK_SEL = 0;  // derive clock from divided pre-muxed ipu1 di0 clock

            HW_CCM_CHSCCDR.B.IPU1_DI0_PODF = 5; // div by 6

            HW_CCM_CHSCCDR.B.IPU1_DI0_PRE_CLK_SEL = 5;  // derive clock from 540M PFD

            //config PFD1 of PLL3 to be 445MHz 

            BW_CCM_ANALOG_PFD_480_PFD1_FRAC(0x13);

            break;

        default:

            printf("the hdmi pixel clock is not supported!\n");

    }

1.png

The resulting clock is 445MHz / 6 = 74.2MHz for 1080p60 and 720p60.

Is that right ??? Why ipu1_di0 clock divider is not set to 3 for 1080p60 ?

Labels (2)
0 Kudos
Reply
1 Reply

2,692 Views
igorpadykov
NXP Employee
NXP Employee

HI Vadim

seems SDK was not tested with 1080p60 so there are no

codes for it. You can add suitable coefficient yourself and test.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply