Core spec detail

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Core spec detail

Jump to solution
3,680 Views
ko-hey
Senior Contributor II

Hi all

Do you have NXP official data of following spec ?

I want to compare the spec by devices.

1. Cortex-A8 Core (i.MX515:800MHz)
 ***mW/MHz
   ***DMIPS/MHz
   ***DMIPS/mW

2. Cortex-A7 Core (i.MX7Solo:800MHz)

   ***mW/MHz

   ***DMIPS/MHz
   ***DMIPS/mW

3. Cortex-A7 Core (i.MX6ULL:792MHz)
 ***mW/MHz
   ***DMIPS/MHz
   ***DMIPS/mW

Ko-hey

Labels (5)
Tags (2)
0 Kudos
Reply
1 Solution
3,387 Views
b36401
NXP Employee
NXP Employee

We have no more information locally.

However we can ask Design Team if they have such details. Please create a technical case:
https://community.nxp.com/thread/381898

View solution in original post

0 Kudos
Reply
4 Replies
3,387 Views
b36401
NXP Employee
NXP Employee

We have following efficiency data (DMIPS/MHz):

A7 core (i.MX6: UL and ULL, i.MX7x) -- 1.9 DMIPS/MHz
A8 core (i.MX 5x) -- 2.01 DMIPS/MHz
A9 core (i.MX6 except UL and ULL) -- 2.5 DMIPS/MHz

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,387 Views
ko-hey
Senior Contributor II

Hi Viktor Linnik

Thank you for sharing the data.

Do you have other data which means DMIPS/MHz and DMIPS/mW ?

Ko-hey

0 Kudos
Reply
3,388 Views
b36401
NXP Employee
NXP Employee

We have no more information locally.

However we can ask Design Team if they have such details. Please create a technical case:
https://community.nxp.com/thread/381898

0 Kudos
Reply
3,387 Views
ko-hey
Senior Contributor II

Hi b36401‌

I made case #001129.

Could you follow and ask to the Design Team ?

Ko-hey

0 Kudos
Reply