Core performance difference between single core ad dual core on i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Core performance difference between single core ad dual core on i.MX6

1,814 Views
Norihiro
Senior Contributor III

Hi,

I'm looking for benchmark test result which was captured on single core version of i.MX6 and dual core version of i.MX6, focusing on A9 core performance itself.

I can find some benchmark test results on i.MX6 Solo and dual cores(http://2014ftf.ccidnet.com/pdf/0058.pdf). But that benchmark is focusing on multimedia performance and hardware acceleration can affect the result.


I want to see benchmark test result using core intensive benchmark program on both dual core and single core.

Could someone advise me if I can find such benchmark test result on the internet?

Thanks,

Norihiro Michigami

0 Kudos
Reply
1 Reply

1,501 Views
igorpadykov
NXP Employee
NXP Employee

HI Norihiro

one can look at Coremark for Quad: 10370@4 cores, 10370/4 per core

EEMBC -- The Embedded Microprocessor Benchmark Consortium

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply