Controlling the Write Address When Writing Image to External Memory

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Controlling the Write Address When Writing Image to External Memory

1,494 Views
samxiao
Contributor I

I have questions about controlling the address of i.MX6 dual lite (the one with EPDC controller in it) when writing an image of 1600x2400 to external memory. Which module is in charge of generating the write image address? SDMA or MMDC? Can either of this module generate 2D address which line offset exists between image lines?

Labels (1)
0 Kudos
Reply
1 Reply

1,430 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sam

PXP module has own dma engine and it provides data processing

for EPDC.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply